Password

Description

In the password settings in PolyScope X, you can find three different passwords.

Protected area What it unlocks Default password

Operational Mode

Switching between Manual and Automatic mode. operator

Safety

Safety settings and the safety configuration. ursafe

Admin

Security screens: Secure Shell, Permissions, and Services. easybot

 

It is possible to set the same password in all three instances, but it is also possible to set three different passwords to separate access and options.

The default passwords are publicly available. To prevent unauthorized access, change the default passwords before operating the system or connecting it to a network.