UR Connect

Connect PolyScope X to myUR Cloud

You have to connect your PolyScope X software to the myUR Cloud service.

You need to find you PIN code in your myUR account.

  1. Go to the Settings tab.

  2. Go to the URConnect tab.

  3. Tap the Connect button on the main UR Connect page.

  4. Add your PIN code from myUR.

When you see the green icon in the right corner of the window, you are connected to the myUR Cloud.

Unsuccessful connect

If you see the "Incorrect PIN code", please review your PIN code from myUR.

 

Diagnostics

If you experience any unexpected when the UR Connect is active, you can go to the Diagnostics.

  1. Go to the Settings tab.

  2. Go to the URConnect tab.

  3. Tap the kebab menu in the top right corner.

  4. Select the Diagnostics option.

 

Export logs

It is possible to export the UR Connect logs from your PolyScope X software.

  1. Go to the Settings tab.

  2. Go to UR Connect.

  3. Tap the kebab menu in the top right corner.

  4. Select the Export Logs option.

  5. Select Export to myUR or Export to USB.