Password - Operational Mode

Default Password

The default password for operational mode: operator.

If you forget your password, it cannot be replaced or recovered.

You will have to reinstall the software.

You must use the default password when you change the password for the first time.

 

Change Operational Mode password

This is how you change the password for operational mode in the PolyScope X setting.

  1. Tap the hamburger menu in the main navigation.

  2. Tap Settings.

  3. Tap Operational Mode in the Password section.

  4. Add the default password, if it is the first time.

  5. Add your preferred password of at least 8 characters.

    Changing the Operational mode password