Transport Without Packaging

Description

Universal Robots always recommends transporting the robot in its original packaging.

These recommendations reduce unwanted vibrations in joints and brake systems and reduce joint rotation.

If you transport the robot without its original packaging, follow these guidelines:

  • Fold the robot as much as possible – do not transport the robot in the singularity position.

  • Move the center of gravity of the robot as close to the base as possible.

  • Secure each tube to a solid surface on two different points on the tube.

  • Secure any attached end effector rigidly in 3 axes.

Transport

Fold the robot as much as
possible.

Do not transport extended.
(singularity position)

Secure the tubes to a solid
surface.

Secure attached end effector in 3 axes.