Backdrive

 

If the robot arm is close to colliding with something, you can use the backdrive function to move the robot arm to a safe position before (re)initializing it.

  1. Press On to enable power. Status changes to Robot Active.

    NEW IMAGES

    Robot status and payload information in the teach pendant.

  2. Press and hold Freedrive. Status changes to Backdrive, as shown in figure 3.6.

     

    NEW IMAGE

     

    3PE TP

    Freedriving a standard TP and 3PE TP.

    The robot arm is “heavy” to move around in Backdrive, so efort is required to move the joints.
    You must test Backdrive mode on all joints.
  3. Move robot as in Freedrive. Joint brakes are released where needed once the Freedrive button is activated.

  Safety settings

Verify the robot safety settings comply with the robot installation risk assessment.

Additional safety inputs and outputs are still functioning

Check which safety inputs and outputs are active and that they can be triggered via PolyScope or external devices.

Backup data See section Backup of Data