Create a Bootable Storage Device

Description

Create a bootable storage device so you can boot a Control Box with a new robot image in either PolyScope version. Use this for recovery if the robot's internal storage is damaged.

 

Download and install balenaEtcher

This procedure uses the open-source flashing tool balenaEtcher to create a storage device with PolyScope installed. You can also use other programs, such as Rufus.

Follow the instructions on the balenaEtcher website to install the program. Go to https://etcher.balena.io/.

balenaEtcher is third-party software and is not associated with Universal Robots A/S. Universal Robots takes no responsibility for this software.

When you successfully install balenaEtcher, its icon appears on your desktop with your other programs.