motion_version_set(version)
Set which Motion Version will be used for movej and movel motion planning.
This command overrides the PolyScope GUI "Installation → Motion → Motion Version → Motion Version 2" setting.
Parameters:
version: 1 or 2. See Motion Version for details.
Example command: motion_version_set(2)
-
Example Parameters:
version = 2 → movej and movel perform as motion version 2
Motion version 1 has identical motion profiles to prior versions of PolyScope
New robot models as well as PolyScope X only support motion version 2