|
The operator needs to have a clear understanding about what the e-Stop on the Teach Pendant affects when pressed.
For example there can be confusion with a multi-robot installation.
It should be made clear if the e-Stop on the Teach Pendant stops the whole installation or only its connected robot.
If there could be confusion, store the Teach Pendant such that the e-Stop button is not visible or usable.
|