Robot Connections: Base Flange Cable
| Description |
This subsection describes the connection for a robot arm configured with a Base Flange Cable connector.
|
|
Base Flange Cable connector |
The Base Flange Cable establishes the robot connection to robot arm to the Control Box. The Robot Cable connects to the Base Flange Cable connector on one end, and to the Control Box connector on the other end. You can lock each connector when robot connection is established. Improper robot connection can result in loss of power to the robot arm.
Connecting the Base Flange Cable directly to any Control Box can result in equipment or property damage.
|