simulator_fault_clear()
Clears a simulated safety system fault in URSim that was triggered by simulator_fault().
This function is available in URSim only. It is not supported on a physical robot controller.
simulator_fault_clear() can only be called from a Secondary Programs while the robot is in ROBOT_MODE_RUNNING or ROBOT_MODE_POWER_OFF.
Parameters
None
Return Value
None
Example command:
sec recover_simulated_fault(): simulator_fault_clear() end