Permissions

Description

Access to the Networking, URCap Management and Updating PolyScope X screens is restricted by default, to prevent unauthorized changes to the system. You can change the permission settings to allow access to these screens. An Admin password is required to access Permissions.

 

To access Permissions
  1. Access the Hamburger menu and select Settings.

  2. Navigate to Security and tap Permissions.

 

Additional system permissions

You can also lock a few important screens/functionalities with the Admin password. On the Permissions screen in Security section in the Settings menu, it is possible to specify which additional screens are to be protected by the Admin password and which screens are available to all users. The following screens/functionalities can optionally be locked:

  • Network settings

  • Update settings

  • URCaps section in the System Manager

  • UR Connect

 

To enable/disable system permissions
  1. Access Permission as previously described. The protected screens are listed under Permissions.

  2. For the desired screen, slide the On/Off toggle switch to the On position to enable it.

  3. To disable the desired screen, slide the On/Off toggle switch to the Off position.

The screen locks again once the toggle is in the Off position.