Robot Cables
| Description |
This section lists the e‑Series robot cables and warns against improper cable selection and the use of incompatible cables.
|
|
The "Standard (black)" and "High flex e-Series (blue)" cables are not compatible with UR20 and UR30 robots.
Conducting installation and/or maintenance of equipment connected to a power source can result in injury or death due to electric shock.
Improper cable selection, usage, or connections can result in loss of power to the robot arm.
Connecting the Base Flange cable directly to any Control Box can result in damage to equipment and property.
Failure to use the robot in accordance with the intended use can result in hazardous situations.
|
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||