modbus_set_runstate_dependent_choice(signal_name, runstate_choice)
Using this method assigns the output to one of the states. This will set the output signal level depending on the state.
Parameters
signal_name:
A string identifying a digital or register output signal that in advance has been added. Can not be empty.
state:
0: Preserve signal state,
1: Set signal Low when program is not running,
2: Set signal High when program is not running,
3: Set signal High when program is running and low when it is stopped,
4: Set signal Low when program terminates unscheduled,
5: Set signal High from the moment a program is started and Low when a program terminates unscheduled,
6: Set signal High when the robot has drive power,
7: Set signal Low when the robot has drive power.
Note: An unscheduled program termination is caused when a Protective stop, Fault, Violation or Runtime exception occurs.
Example command:
modbus_set_runstate_dependent_choice("output2", 3)
-
Example Parameters:
-
Signal name = output2
-
Runstate dependent choice = 3 ! set Low when a program is stopped and High when a program is running
-