Compute Module

Description

AI Accelerator includes Compute module based on NVIDIA Jetson Orin.

Read the NVIDIA Jetson Orin manual and follow all safety instructions.

Compute Module position

When positioning the Compute Module, ensure the following:

  • The Compute Module is placed in a clean and dry space with sufficient airflow.
  • The cable from the 3D camera can reach the Compute Module.

Connecting Compute Module

The Compute Module network connections are pre-configured with Lan1 designated for connecting to the robot's Control Box and Lan2 available for optional Internet connection.

 

Connect the port marked Lan1 on the Compute Module directly to the robot's Control Box with an Ethernet cable. Do not use router or switch.

Initial software setup on the Compute Module will require monitor, keyboard and mouse.