Certifications

Description

This section contains information about certificates and declarations valid for Universal Robots robots with OEM controllers.

Shipping materials

As stated by our suppliers, Universal Robots robots shipping materials comply with the ISPM-15 requirements for producing wood packaging material and are marked accordingly.

Certification of quality Universal Robots robots undergo continuous internal testing and end-of-line test procedures. UR testing processes undergo continuous review and improvement.
Declarations according to EU directives

Universal Robots robots are certified according to the following directives.

  • 2006/42/EC – Machinery Directive (MD)
    According to the Machinery Directive 2006/42/EC, Universal Robots robots are partly completed machinery, and do not have a CE mark on them.
  • 2012/19/EU – Waste of Electrical and Electronic Equipment (WEEE)
    For information on disposal of electrical and electronic equipment waste, refer to chapter 7, Disposal and Environment in the robot user manual.