Unlock Safety Settings

Description

You have to unlock the safety settings to change them.

Safety Settings are password protected.

The default password for safety: ursafe.

Unlock safety settings
  1. In the PolyScope X Main Navigation, tap the Application tab.

  2. On the workcell screen tap the Safety icon.

  3. Observe that the Robot Limits screen displays, but settings are inaccessible.

  4. Enter the safety password and tap UNLOCK to make settings accessible.

  5. Tap LOCK or navigate away from the Safety menu to lock all Safety item settings again.