|
The safety system limits are defined in the Safety Configuration.
The safety system receives values from the input fields and detects any violation if any the values are exceeded.
The robot controller prevents violations by making a robot stop or by reducing the speed.
Use of Safety Configuration parameters different from those defined by the risk assessment can result in hazards that are not reasonably eliminated or risks that are not sufficiently reduced.
|