Remote ON/OFF Control and Emergency Stop

Description

The OEM Control Box requires a remote ON/OFF control and an emergency stop push-button. The following sections describe how to install them using the I/O ports.

 

Connecting the ON/OFF Control

 

The images below shows how the remote ON/OFF control is connected.

1 Status: On 2 Status: Off

Connecting the Remote Emergency Stop

Description

Install an external Emergency Stop (E-stop) if the Teach Pendant with the default Emergency Stop is not connected to the Control Box.

 

The following illustration shows the minimum required Emergency Stop installation.