Safety Configuration

Safety Settings are password protected.

  1. In the PolyScope X Main Navigation, tap the Application tab.

  2. On the workcell screen tap the Safety icon.

  3. Observe that the Robot Limits screen displays, but settings are inaccessible.

  4. Enter the safety password and tap UNLOCK to make settings accessible. The default password for safety: ursafe. Note: Once Safety settings are unlocked, all settings are now active.

  5. Tap LOCK or navigate away from the Safety menu to lock all Safety item settings again.