Round Sling Use

Description

The round sling is provided by UR with UR Series robots.

According to the manufacturer, the round sling conforms to the following standards:

  • EN 1492-1 :2000+A1 :2008 Textile slings - Safety - Flat woven webbing slings, made of man-made fibers, for general purpose use.

  • EN 1492-2 :2000+A1 :2008 Textile slings - Safety - Round slings, made of man-made fibers, for general purpose use.

 

Using the round sling without an inspection can lead to injury.

  • Inspect the sling before and after each use.

  • Inspect the sling during use if possible.

 

Using a damaged round sling can result in injury.

  • Carefully examine the sling visually before each use.

  • Do not use the sling if it is cracked, ripped, or the stitching is loose.

  • Do not use the sling if there are signs of heat damage.

 

Incorrect storage and/or handling can cause damage to the round sling.

  • Keep the sling away from acids and bases.

  • Protect the sling against sharp edges and friction.

  • Do not tie a knot in the sling.

 

There may be specific regulations for inspecting lifting equipment in your region.

  • Observe local regulations regarding inspection of lifting equipment.

  • Observe local regulations regarding inspection frequency of lifting equipment.

Table
  Round Sling Description
Item Round sling 1T x 1M/2M    
Color Violet (according to EN 1492-2)    
Material Polyester    
WLL Factor 1.0 (1000 KG) Straight Lift

0.8 (800 KG) Choke Hitch