Functions

Process data exchanged through the connection assembly instances is accessible using read and write handle objects in the robot program. Typically handle would be opened once and data layout will be defined in the "Before Start" section (or by script contributed from URCap). Afterwards individual reads and writes can be executed with methods on the configured handles.

eip_reader_factory(instance_name, data_size)

Opens handle to PLC→Robot data. Typically placed in the "Before Start" section of the program.

instance_name: A string, or an integer instance id.

data_size: An integer, instance data size in bytes.

handle object The handle provides a read only access to the instance data.

Example global cnc_status = eip_reader_factory(111, 44)

Opens the handle to PLC→Robot instance with an id 111, and data size 44 bytes. Handle is saved into cnc_status global variable.

eip_writer_factory(instance_name, data_size)

Opens handle to Robot→PLC data. Typically placed in "Before Start" section of the program.

instance_name: A string, or an integer instance id.

data_size: An integer, instance data size in bytes.

handle object The handle provides a write only access to the instance data.

Example global cnc_command = eip_writer_factory(101, 88)

Opens the handle to Robot→PLC instance with an id 101, and data size 88 bytes. Handle is saved into cnc_command global variable.

Methods on reader and writer handles

Handles are used to define underlying assembly memory layout, and later read and write process data.

Methods are invoked on handles using '.' operator. Methods are grouped in 2 families:

define_...(offset, data_name) - numeric fields

Family of functions defining single numeric field.

Methods define individual labels in assembly instances exchanged with PLC. Labels are later used by read, and write methods.

NOTE: Overlapping data definitions are not allowed, except for overlap with bit fields.

offset: An integer, position of the data in the instance in bytes.

data_name: A string, label.

Example cnc_status.define_uint8(11, "service_code")

Set label "service_code" to single byte at offset 11.

define_bit(offset, bit_number, data_name, bitfield_width=1)

Method defines individual label in the assembly instance exchanged with PLC. Label is later used by read, and write methods.

NOTE: Overlapping bit definitions are not allowed, except for overlap with numeric fields.

offset: An integer, position of the data in the instance in bytes.

bit_number : An integer, bit number in a word. 0 = least significant bit. Depending on the bitfield_width most significant bit will be 7, 15, or 31.

data_name: A string, label.

bitfield_width: An integer, can be 1, 2 or 4 representing bit in byte, word, or double word. (Optional)

Example 1 cnc_status.define_bit(0, 0, "comm_check")

Set label "comm_check" to bit 0 in byte 0.

Example 2 cnc_status.define_bit(16, 9, "door_opened", 2)

Set label "door_opened" to bit 9 in word starting on byte 16.

define_..._array(offset, length, data_name) - arrays of numeric fields

Family of functions defining arrays of numeric fields.

Methods define individual labels in assembly instances exchanged with PLC. Labels are later used by read, and write methods.

NOTE: Overlapping data definitions are not allowed, except for overlap with bit fields.

offset: An integer, position of the data in the instance in bytes.

length: An integer, number of elements of the array with base size specified by the data type (e.g. for define_uint16_array length = 4 will use 8 bytes).

data_name: A string, label.

Example 1 cnc_command.define_uint8_array(48, 32, "work_number")

set label "work_number" to 32 byte long array starting at byte 48.

Example 2 cnc_command.define_int16_array(120, 3, "axes_offset")

Set label "axes_offset" to 3 words (6 byte long) array starting at byte 120.

define_string(offset, length, data_name)

Method defines individual label in the assembly instance exchanged with PLC. Label is later used by read, and write methods.

NOTE: Overlapping data definitions are not allowed.

offset: An integer, position of the data in the instance in bytes.

length: An integer, number of characters in the string. String should be terminated with 0 if it's shorter than length.

data_name: A string, label.

Example cnc_command.define_string(200, 32, "program_name")

Set label "program_name" to up to 31 character long string starting at byte 200. Space should be left for termination null character.

read(data_names)

Method reads one or more data labels written by external PLC. Latest data is read from internal buffer.

data_names:

Depending on the parameter method returns basic type, or complex type (struct with named fields)

Example 1 comm_check = cnc_status.read("comm_check")

Reads single bit to comm_check URScript variable.

Example 2 service_request = cnc_status.read(["door_closed", "service_code"])

Reads multiple fields that can be accessed as service_request struct members.

Individual basic types can be extracted from struct with '.' operator: service_request.door_closed, service_request.service_code

write(data_struct)

Method writes one or more data labels to memory read by external PLC.

All labels in struct are guaranteed to be written at the same time to the assembly instance data.

NOTE: method will check values based on the type of the data label. Numbers exceeding data type will stop a program with runtime exception.

data_struct:Struct where member names are data labels, and values are data contents

Example 1 cnc_command.write(struct(work_number = [1, 2, 3, 4], search_start = True))

Set work_number label array, and search_start bit.

Example 2 cnc_command.write(struct(door_open = True))

Set single bit with "door_open" label.

Example 3

s = struct(robot_ready = False, machine_stop = False, robot_alarm = False)
s.robot_ready = True
cnc_command.write(s)

Define global struct, and reuse in calls to write method.

write(data_name, value)

Introduced in Software 5.22.0/10.10.0.

Method writes one data label to memory read by external PLC.

NOTE: method will check value based on the type of the data label. Numbers exceeding data type will stop a program with runtime exception.

data_name:String, data label to write.

value:Value for an output instance. Type depends on data_name definition.

Example cnc_command.write("door_open", True))

Set single bit with "door_open" label.

clear()

Method sets all memory managed by write handle to zero.

set_watchdog(frequency, action)

Registers a new watchdog on the handle. This can only be called on a read handle. After the call, the new watchdog will start immediately.

Calling multiple times on the same handle reconfigures watchdog with new parameters.

frequency: A float, minimum allowed communication frequency. Allowed values are greater then 0 and lower or equal to 10 Hz. Fractional frequencies are allowed.

action : An integer

Example cnc_status.set_watchdog(2.5, 1)

Pause program if no data was received from master for more than 400ms.

start_watchdog()

Method starts the watchdog. Throws a runtime error if watchdog is not registered.

NOTE: Watchdog starts automatically when it's created. This function can be used in combination with stop_watchdog().

stop_watchdog()

Method disables the watchdog. Throws a runtime error if watchdog is not registered.

This method can be used to temporarily mute watchdog.

close()

Method closes handle object, and frees memory associated. It's recommended to close handles if they are used only once in a program. If handle is used repeatedly then it's recommended to keep it open over the lifespan of the program.

NOTE: The same handle can not be opened again, new handle has to be created.