External Device Connection Ports

Description

The bottom side of the OEM Control Box contains a bracket with ports for connecting external devices. The following illustration shows the bracket.

1 Teach Pendant port 2 SD card slot
3 Ethernet port 4 USB ports
5 Mini Displayport 6 10 A mini blade fuse
Port Description
Teach Pendant The port for connecting the Teach Pendant (Teach Pendant sold separately).
Ethernet Connect external devices supporting MODBUS, Ethernet/IP, or PROFINET.
USB ports Connect USB devices, for example a mouse, keyboard, a USB flash drive.
Mini Displayport

Connect a monitor. The output video stream shows the same as the display on the Teach Pendant. Supported connection types:

  • DP (direct connection).
  • Active DVI (using an active DP to DVI converter).
  • Active HDMI (using an active DP to HDMI converter).
10 A mini blade fuse Connect a fuse. The fuse must be UL-marked and have a 10 A current rating.
SD card The SD card is already in the SD card port.
Removing the SD card under operation can corrupt the system. Do not remove the SD card.
Connecting a Keyboard or Monitor

Use a USB port to connect a keyboard.

Use the Mini Displayport to connect a monitor.

You cannot connect a mouse when using PSX software.
Connecting a Teach Pendant

You can only use the OEM PSX Control Box with a Teach Pendant (TP) or 3PE Teach Pendant (3PE TP).