high_holding_torque_enable()
Enables high hold torque when the robot is stationary. This function is used to reverse the behavior of the high_holding_torque_disable() command.
Parameters:
None
Example command:
high_holding_torque_enable()
See also
high_holding_torque_disable()