encoder_enable_set_tick_count(encoder_index, range_id)
Sets up an encoder expecting to be updated with tick counts via the function encoder_set_tick_count.
>>> encoder_enable_set_tick_count(0,0)
This example shows how to set up encoder 0 to expect counts in the range of [-2147483648 ; 2147483647].
Parameters
encoder_index:
Index of the encoder to define. Must be either 0 or 1.
range_id:
decoder_index: Range of the encoder
(integer). Needed to handle wrapping nicely.
0 is a 32 bit signed encoder, range [-2147483648 ; 2147483647]
1 is a 8 bit unsigned encoder, range [0 ; 255]
2 is a 16 bit unsigned encoder, range [0 ; 65535]
3 is a 24 bit unsigned encoder, range [0 ; 16777215]
4 is a 32 bit unsigned encoder, range [0 ; 4294967295]