Real-Time Data Exchange (RTDE)

The RTDE synchronize external executables with the UR controller, for instance Ethernet IP, without breaking any real-time properties.

Introduction

The Real-Time Data Exchange (RTDE) interface provides a way to synchronize external applications with the UR controller over a standard TCP/IP connection, without breaking any real-time properties of the UR controller. This functionality is among others useful for interacting with drivers (e.g. Ethernet/IP), manipulating robot I/O and plotting robot status (e.g. robot trajectories). The RTDE interface is by default available when the UR controller is running.

The synchronization is configurable and can for example involve the following data:

  • Output: robot-, joint-, tool- and safety status, analog and digital I/O's and general purpose output registers

  • Input: digital and analog outputs and general purpose input registers

The RTDE functionality is split in two stages: a setup procedure and a synchronization loop.

On connection to the RTDE interface, the client is responsible for setting up the variables to be synchronized. Any combination of input and output registers that the client needs to write and read, respectively, can be specified. To achieve this the client sends a setup list of named input and output fields that should be contained in the actual data synchronization packages. The definition of a synchronization data package format is referred to as a recipe. There is a maximum limit of 2048 bytes to represent the list of inputs/outputs field names a client would like to subscribe to. In return the RTDE interface replies with a list of the variable types or specifies that a specific variable has not been found. Each input recipe that has been successfully configured will get a unique recipe id. The list of supported field names and their associated data types can be found below. When the setup is complete the data synchronization can be started and paused.

When the synchronization loop is started, the RTDE interface sends the client the requested data in the same order it was requested by the client. Furthermore the client is expected to send updated inputs to the RTDE interface on a change of value. The data synchronization uses serialized data.

All packages share the same general structure with a header and a payload if applicable. The packages used for the setup procedure generate a return message. The synchronization loop packages do not. Both client and server may at any time send a text message, whereby the warning level specifies the severity of the problem. The RTDE is available on port number 30004.

To get started we recommend to use or modify the provided client sample written in Python.

Key features

  • Real-time synchronization: The RTDE generally generates output messages on 125 Hz. However, the real-time loop in the controller has a higher priority than the RTDE interface. Therefore, if the controller lacks computational resources it will skip a number of output packages. The skipped packages will not be sent later, the controller will always send the most recent data. Input packages will always be processed in the control cycle they are received, so the load for the controller will vary depending on the number of received packages.
  • Input messages: The updating of variables in the controller can be divided into multiple messages. One can have one message to update everything or a message per variable or any division in between. There is no need for a constant update rate; inputs keep their last received value. Note: Only one RTDE client is allowed to control a specific variable at any time.
  • Runtime environment: An RTDE client may run on the UR Control Box PC or on any external PC. The advantage of running the RTDE client on the Control Box is no network latency. However, the RTDE client and UR controller will compete for computational resources. Please make sure that the RTDE client runs with standard operating system priority. Computationally intensive processes, e.g. image processing, should be run on an external PC.
  • Protocol changes: The RTDE protocol might be updated at any time by UR. To guarantee maximum compatibility for your RTDE client, RTDE clients can request the RTDE interface to speak a specific protocol version. Protocol additions / changes are explicitly denoted, otherwise version 1 is assumed.

Field names and associated types

Robot controller inputs

Name Type Comment Introduced in version
speed_slider_mask UINT32

0 = don't change speed slider with this input

1 = use speed_slider_fraction to set speed slider value


speed_slider_fraction DOUBLE new speed slider value
standard_digital_output_mask UINT8 Standard digital output bit mask
configurable_digital_output_mask UINT8

Configurable digital output bit mask


standard_digital_output UINT8 Standard digital outputs
configurable_digital_output UINT8 Configurable digital outputs
standard_analog_output_mask UINT8

Standard analog output mask

Bits 0-1: standard_analog_output_0 | standard_analog_output_1


standard_analog_output_type UINT8

Output domain {0=current[mA], 1=voltage[V]}

Bits 0-1: standard_analog_output_0 | standard_analog_output_1


standard_analog_output_0 DOUBLE Standard analog output 0 (ratio) [0..1]
standard_analog_output_1 DOUBLE Standard analog output 1 (ratio) [0..1]
input_bit_registers0_to_31 UINT32

General purpose bits

This range of the boolean input registers is reserved for FieldBus/PLC interface usage.


input_bit_registers32_to_63 UINT32

General purpose bits

This range of the boolean input registers is reserved for FieldBus/PLC interface usage.


input_bit_register_X BOOL

64 general purpose bits

X: [64..127] - The upper range of the boolean input registers can be used by external RTDE clients (i.e URCAPS).

3.9.0 / 5.3.0
input_int_register_X INT32

48 general purpose integer registers
X: [0..23] - The lower range of the integer input registers is reserved for FieldBus/PLC interface usage.

X: [24..47] - The upper range of the integer input registers can be used by external RTDE clients (i.e URCAPS).

[0..23] 3.4.0

[24..47] 3.9.0 / 5.3.0

input_double_register_X DOUBLE

48 general purpose double registers

X: [0..23] - The lower range of the double input registers is reserved for FieldBus/PLC interface usage.

X: [24..47] - The upper range of the double input registers can be used by external RTDE clients (i.e URCAPS).

[0..23] 3.4.0

[24..47] 3.9.0 / 5.3.0

external_force_torque VECTOR6D Input external wrench when using ft_rtde_input_enable builtin. 3.3

Robot controller outputs

Name Type Comment

Introduced

in version

timestamp DOUBLE Time elapsed since the controller was started [s]
target_q VECTOR6D Target joint positions
target_qd VECTOR6D Target joint velocities
target_qdd VECTOR6D Target joint accelerations
target_current VECTOR6D Target joint currents
target_moment VECTOR6D Target joint moments (torques)
actual_q VECTOR6D Actual joint positions
actual_qd VECTOR6D Actual joint velocities
actual_current VECTOR6D Actual joint currents
joint_control_output VECTOR6D Joint control currents
actual_TCP_pose VECTOR6D Actual Cartesian coordinates of the tool: (x,y,z,rx,ry,rz), where rx, ry and rz is a rotation vector representation of the tool orientation
actual_TCP_speed VECTOR6D Actual speed of the tool given in Cartesian coordinates
actual_TCP_force VECTOR6D Generalized forces in the TCP
target_TCP_pose VECTOR6D Target Cartesian coordinates of the tool: (x,y,z,rx,ry,rz), where rx, ry and rz is a rotation vector representation of the tool orientation
target_TCP_speed VECTOR6D Target speed of the tool given in Cartesian coordinates
actual_digital_input_bits UINT64 Current state of the digital inputs.
joint_temperatures VECTOR6D Temperature of each joint in degrees Celsius
actual_execution_time DOUBLE Controller real-time thread execution time
robot_mode INT32

Robot mode


joint_mode VECTOR6INT32

Joint control modes


safety_mode INT32 Safety mode
safety_status INT32 Safety status 3.10.0 / 5.4.0
actual_tool_accelerometer VECTOR3D Tool x, y and z accelerometer values
speed_scaling DOUBLE Speed scaling of the trajectory limiter
target_speed_fraction DOUBLE Target speed fraction
actual_momentum DOUBLE Norm of Cartesian linear momentum
actual_main_voltage DOUBLE Safety Control Board: Main voltage
actual_robot_voltage DOUBLE Safety Control Board: Robot voltage (48V)
actual_robot_current DOUBLE Safety Control Board: Robot current
actual_joint_voltage VECTOR6D Actual joint voltages
actual_robot_energy_consumed DOUBLE

Robot Arm energy consumption since controller startup [Wh].

5.24.0 / 10.11.0
actual_robot_energy_produced DOUBLE

Robot Arm energy production during regenerative braking, since controller startup [Wh].

This energy is flowing back into the Control Box and gets dissipated as heat.

5.24.0 / 10.11.0
actual_digital_output_bits UINT64 Digital outputs
runtime_state UINT32 Program state
elbow_position VECTOR3D Position of robot elbow in Cartesian Base Coordinates
3.5.0 / 5.0.0
elbow_velocity VECTOR3D Velocity of robot elbow in Cartesian Base Coordinates
3.5.0 / 5.0.0
robot_status_bits UINT32

Bits 0-3:  Is power on | Is program running | Is teach button pressed | Is power button pressed


safety_status_bits UINT32

Bits 0-10: Is normal mode | Is reduced mode | Is protective stopped | Is recovery mode | Is safeguard stopped | Is system emergency stopped | Is robot emergency stopped | Is emergency stopped | Is violation | Is fault | Is stopped due to safety


analog_io_types UINT32
Bits 0-3: analog input 0 | analog input 1 | analog output 0 | analog output 1, {0=current[mA], 1=voltage[V]}

standard_analog_input0 DOUBLE Standard analog input 0 [mA or V]
standard_analog_input1 DOUBLE Standard analog input 1 [mA or V]
standard_analog_output0 DOUBLE Standard analog output 0 [mA or V]
standard_analog_output1 DOUBLE Standard analog output 1 [mA or V]
io_current DOUBLE I/O current [mA]
encoder0_raw INT32
Raw encoder0 counter counter with range of [-2³¹, 2³¹[

encoder1_raw INT32
Raw encoder1 counter with range of [-2³¹, 2³¹[

euromap67_input_bits UINT32
Euromap67 input bits

euromap67_output_bits UINT32
Euromap67 output bits

euromap67_24V_voltage DOUBLE
Euromap 24V voltage [V]

euromap67_24V_current DOUBLE
Euromap 24V current [mA]

tool_mode UINT32 Tool mode
tool_analog_input_types UINT32

Output domain {0=current[mA], 1=voltage[V]}

Bits 0-1: tool_analog_input_0 | tool_analog_input_1


tool_analog_input0 DOUBLE Tool analog input 0 [mA or V]
tool_analog_input1 DOUBLE Tool analog input 1 [mA or V]
tool_output_voltage INT32 Tool output voltage [V]
tool_output_current DOUBLE Tool current [mA]
tool_temperature DOUBLE Tool temperature in degrees Celsius
tcp_force_scalar DOUBLE TCP force scalar [N]
joint_position_deviation_ratio DOUBLE
wrench_calc_from_currents VECTOR6D The forces and torques derived from the joint currents
output_bit_registers0_to_31 UINT32 General purpose bits
output_bit_registers32_to_63 UINT32 General purpose bits
output_bit_register_X BOOL

64 general purpose bits

X: [64..127] - The upper range of the boolean output registers can be used by external RTDE clients (i.e URCAPS).

3.9.0 / 5.3.0
output_int_register_X INT32

48 general purpose integer registers

X: [0..23] - The lower range of the integer output registers is reserved for FieldBus/PLC interface usage.

X: [24..47] - The upper range of the integer output registers can be used by external RTDE clients (i.e URCAPS).

[0..23] 3.4.0

[24..47] 3.9.0 / 5.3.0

output_double_register_X DOUBLE

48 general purpose double registers

X: [0..23] - The lower range of the double output registers is reserved for FieldBus/PLC interface usage.

X: [24..47] - The upper range of the double output registers can be used by external RTDE clients (i.e URCAPS).

[0..23] 3.4.0

[24..47] 3.9.0 / 5.3.0

input_bit_registers0_to_31 UINT32

General purpose bits (input read back)

This range of the boolean output registers is reserved for FieldBus/PLC interface usage.

3.4.0
input_bit_registers32_to_63 UINT32

General purpose bits (input read back)

This range of the boolean output registers is reserved for FieldBus/PLC interface usage.

3.4.0
input_bit_register_X  ([64 .. 127]) BOOL

 64 general purpose bits

X: [64..127] - The upper range of the boolean output registers can be used by external RTDE clients (i.e URCAPS).

3.9.0 / 5.3.0

input_int_register_X  ([0 .. 48])
INT32 48 general purpose integer registers 

X: [0..23] - The lower range of the integer input registers is reserved for FieldBus/PLC interface usage.

X: [24..47] - The upper range of the integer input registers can be used by external RTDE clients (i.e URCAPS).

[0..23] 3.4.0

[24..47] 3.9.0 / 5.3.0

input_double_register_X ([0 .. 48])
DOUBLE  48 general purpose double registers 

X: [0..23] - The lower range of the double input registers is reserved for FieldBus/PLC interface usage.

X: [24..47] - The upper range of the double input registers can be used by external RTDE clients (i.e URCAPS).

[0..23] 3.4.0

[24..47] 3.9.0 / 5.3.0

tool_output_mode UINT8 The current output mode
tool_digital_output0_mode UINT8 The current mode of digital output 0
tool_digital_output1_mode UINT8 The current mode of digital output 1
payload DOUBLE Payload mass Kg
payload_cog VECTOR3D Payload Center of Gravity (CoGx, CoGy, CoGz) m
script_control_line UINT32

Script line number that is actually in control of the robot given the robot is locked by one of the threads in the script.

If no thread is locking the robot this field is set to '0'. Script line number should not be confused with program tree line number displayed on polyscope.

3.14.0 / 5.9.0
actual_current_as_torque VECTOR6D Actual joint currents converted to torques

Data types

Name Type Size in bits
BOOL 0 = False, everything else = True 8

UINT8

unsigned integer 8
UINT32 unsigned integer 32
UINT64 unsigned integer 64
INT32 signed integer, two's complement 32
DOUBLE IEEE 754 floating point 64
VECTOR3D 3xDOUBLE 3x64
VECTOR6D 6xDOUBLE 6x64
VECTOR6INT32 6xINT32 6x32
VECTOR6UINT32 6xUINT32 6x32
STRING ASCII char array lengthx8

Network byte order

Protocol

EE = External Executable

CON = Robot Controller

Output: CON -> EE

Input: CON <- EE

Header

Field name Data Type
package size uint16_t
package type uint8_t

Summary: All packages use the header.

Supported package types are:

Package name Package type ascii equivalent
RTDE_REQUEST_PROTOCOL_VERSION 86 V
RTDE_GET_URCONTROL_VERSION 118 v
RTDE_TEXT_MESSAGE 77 M
RTDE_DATA_PACKAGE 85 U
RTDE_CONTROL_PACKAGE_SETUP_OUTPUTS 79 O
RTDE_CONTROL_PACKAGE_SETUP_INPUTS 73 I
RTDE_CONTROL_PACKAGE_START 83 S
RTDE_CONTROL_PACKAGE_PAUSE 80 P

Direction: Bilateral

Return: Not available

RTDE_REQUEST_PROTOCOL_VERSION

Field name Data Type
Header See above
protocol version uint16_t

Summary: Request the controller to work with "protocol version"

Direction: EE -> CON

Return

Field name Data Type
Header See above
accepted uint8_t

Summary: The controller accepts or not, i.e. either 1 (success) or 0 (failed). On success, the EE should speak the specified protocol version and the CON will answer in that version.

RTDE_GET_URCONTROL_VERSION

Field name Data Type
Header See above

Summary: Retrieves the CON major, minor, bugfix and build number.

Direction: EE -> CON

Return

Field name Data Type
Header See above
major uint32_t
minor uint32_t
bugfix uint32_t
build uint32_t

Summary: The major, minor, bugfix and build number.

RTDE_TEXT_MESSAGE (protocol v. 1)

Direction: CON -> EE

Field name Data Type
Header See above
message type uint8_t
message string

Direction: EE -> CON

Field name Data Type
Header See above
message length uint8_t
message string
source length uint8_t
source string
warning level uint8_t

Summary: Send an exception, error, warning or info message. 

Warning level: EXCEPTION_MESSAGE, ERROR_MESSAGE, WARNING_MESSAGE, INFO_MESSAGE

EE->CON: Exceptions indicate EE program failure without recovery possibilities. Error, warning and info will end up in the PolyScope log.

CON -> EE: Indicates mainly different kinds of protocol failures.

Direction: See above

Return: Not available.

RTDE_TEXT_MESSAGE (protocol v. 2)

Field name Data Type
Header See above
message length uint8_t
message string
source length uint8_t
source string
warning level uint8_t

Summary: Send an exception, error, warning or info message. 

Warning level: EXCEPTION_MESSAGE, ERROR_MESSAGE, WARNING_MESSAGE, INFO_MESSAGE

EE->CON: Exceptions indicate EE program failure without recovery possibilities. Error, warning and info will end up in the PolyScope log.

CON -> EE: Indicates mainly different kinds of protocol failures.

Direction: Bilateral

Return: Not available.

RTDE_DATA_PACKAGE

Field name Data Type
Header See above
recipe id uint8_t
<variable> <data type>

Summary: An update to the CON/EE inputs respectively.

The <variable>s are packaged/serialized binary and match the type specified by the SETUP_OUTPUTS or SETUP_INPUTS requests return.

Direction: Bilateral

Return: Not available

RTDE_CONTROL_PACKAGE_SETUP_OUTPUTS (protocol v. 1)

Field name Data Type
Header See above
variable names string

Summary: Setup the outputs recipe. At the moment the CON only supports one output recipe. The package should contain all desired output variables. The variables names is a list of comma separated variable name strings.

Direction: EE -> CON

Return

Field name Data Type
Header See above
variable types string

Summary: Returns the variable types in the same order as they were supplied in the request.

Variable types: VECTOR6D, VECTOR3D, VECTOR6INT32, VECTOR6UINT32, DOUBLE, UINT64, UINT32, INT32, BOOL, UINT8

If a variable is not available, then the variable type will be "NOT_FOUND".

In case of one or more "NOT_FOUND" return values, the recipe is considered invalid and the RTDE will not output this data.

RTDE_CONTROL_PACKAGE_SETUP_OUTPUTS (protocol v. 2)

Field name Data Type
Header See above
output frequency double
variable names string

Summary: Setup the outputs recipe. At the moment the CON only supports one output recipe and the output frequency is configurable. The frequency must be between 1 and 125 Hz and the output rate will be according to floor(125 / frequency). The package should contain all desired output variables. The variable names is a list of comma separated variable name strings.

Direction: EE -> CON

Return

Field name Data Type
Header See above
output recipe id uint8_t
variable types string

Summary: Returns the variable types in the same order as they were supplied in the request.

Variable types: VECTOR6D, VECTOR3D, VECTOR6INT32, VECTOR6UINT32, DOUBLE, UINT64, UINT32, INT32, BOOL, UINT8

If a variable is not available, then the variable type will be "NOT_FOUND".

In case of one or more "NOT_FOUND" return values, the recipe is considered invalid and the RTDE will not output this data (output recipe id = 0).

RTDE_CONTROL_PACKAGE_SETUP_INPUTS

Field name Data Type
Header See above
variable names string

Summary: Setup a CON input recipe.The CON supports 255 different input recipes (0 is reserved). The variables names is a list of comma separated variable name strings.

Direction: EE -> CON

Return

Field name Data Type
Header See above
input recipe id uint8_t
variable types string

Summary: Returns the variable types in the same order as they were supplied in the request.

Variable types: VECTOR6D, VECTOR3D, VECTOR6INT32, VECTOR6UINT32, DOUBLE, UINT64, UINT32, INT32, BOOL, UINT8

If a variable has been claimed by another EE, then the variable type will be "IN_USE".

If a variable is not available, then the variable type will be "NOT_FOUND".

In case of one or more "IN_USE" or "NOT_FOUND" return values, the recipe is considered invalid (input recipe id = 0).

RTDE_CONTROL_PACKAGE_START

Field name Data Type

Header

See above

Summary: Request the controller to start sending output updates. This will fail if e.g. an output package has not been configured yet.

Direction: EE -> CON

Return

Field name Data Type
Header See above
accepted uint8_t

Summary: The CON accepts or not. Either 1 (success) or 0 (failed).

RTDE_CONTROL_PACKAGE_PAUSE

Field name Data Type
Header See above

Summary: Request the CON to pause sending output updates.

Direction: EE -> CON

Return

Field name Data Type
Header See above
accepted uint8_t

Summary: The CON will always accept a pause command and return a 1 (success).