UR Download

Here you can download a lot of useful files including manuals, drawings, robot software update and more! Select your download from the menus below

Select robot type

Label on the robot arm and control box will show what type it is.

Select type of download for CB-Series

Search for article 17278 for more info on "How to use this Support site"

Select type of software

Robot software should ONLY be installed by trained personnel.
The software is not backwards compatible.

Software is covered under End User Software Licence Agreement. Please find this under software selection.

Select operating system for your computer

URSim is a simulation software intended for offline programming and simulation of both robot programs and manual movement of robot.

NOTE: Not all functions works compared to a real robot, please see below.
- Emergency stop can not be used
- Input IO state can not be set
- Paths are perfect
- Collisions with self or with surrounding objects do not work
- Force mode will not work

Select Software version

The file is ready to download

ursim 3.6.1

URSim on Linux

Installing the Universal Robots simulator software on Linux.

The information on this page applies to software versions 3.3 and newer.

The simulator has been tested on the Linux Mint 17.1 Rebbecca distribution (Ubuntu 14.04 based). Universal Robots gives no guarenties/do not provide any support with respect to the execution of this software on other Linux distributions. 

 

 

Introduction

This mini guide explains how to install the Universal Robots software (GUI and controller) on Ubuntu Linux. 

With this software installed it is possible to create and run programs on a simulated robot, with some limitations. The most important of these limitations is that it is not possible to simulate digital/analogue input to the robot. Furthermore touch screen set-up and network set-up from within the GUI won't work. The robot is able to communicate via TCP/IP, if this is configured on the host machine.

The basic prerequisites for the software is Python 2.6.

  

Install the software

First download the software provided here and save it to your home folder. Change to your home folder and extract the file to the root of your home folder:

cd ~
tar xvzf [FILE NAME]
cd ursim-3.X.X.XXXXX
./install.sh

Now you can simply run the software from the terminal by running:

cd ..
ursim-3.X.X.XXXXX/start-ursim.sh

Or, if your prefer, use the short-cuts created on your desktop.

 

Enable Modbus server in URSim

As per default, the Modbus server is activated. In case it is not then open the file starturcontrol.sh which is located in the installation folder using a file editor.

Modify this line:

HOME=$SCRIPT_DIR $SCRIPT_DIR/URControl &>$SCRIPT_DIR/URControl.log &

into:

echo <linux_password> | sudo -S HOME=$SCRIPT_DIR $SCRIPT_DIR/URControl &>$SCRIPT_DIR/URControl.log &

where password is the login password for Linux

Difficulty: Advanced

Want to get notified about updates?

You are welcome to sign up for notifications about new relevant information and articles that could be interesting for you.

Need help?

Did you find what you needed on this site? For additional information please contact one of our distributors.