public class CannotAccessDeprecatedUserInput extends RuntimeException
This exception is thrown when an attempt is made to access a user input, e.g. reading the value using
UserInput.getValue(), after the user input has been deprecated (using the
CustomUserInputConfiguration.deprecateUserInput(UserInput) method).
CustomUserInputConfiguration.deprecateUserInput(UserInput) method must be used instead.| Constructor and Description |
|---|
CannotAccessDeprecatedUserInput(String message) |
addSuppressed, fillInStackTrace, getCause, getLocalizedMessage, getMessage, getStackTrace, getSuppressed, initCause, printStackTrace, printStackTrace, printStackTrace, setStackTrace, toStringpublic CannotAccessDeprecatedUserInput(String message)
Copyright © 2024. All rights reserved.